Hello,
I am attempting to setup XDC tools in a shared network location as described by section 1.2.1 of the XDC Getting Started Guide. When using the proceedure described here:
http://rtsc.eclipse.org/cdoc-tip/xdc/tools/configuro/ccs/package.html
I got the following error:
Can anyone help me understand what that means? I was unable to find any reference on this forum or on Google.
My ultimate goal is to have one set of the various XDC libraries shared among all developers. Though I have all my environment variables pointing to the correct location, when I try to create a new RTSC project in Code Composer, it claims that XDC tools are not installed. I should also mention that the files are not actually stored on the network at the moment, just in the non-default directory with the original default install removed.
Thanks in advance for any insights,
Richard Zuber