This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: 1920*1080 resolution errors happened in the ""app_tidl" demo

Part Number: TDA4VM

Hi 

    if I set  "#define DISPLAY_WIDTH (1920) #define DISPLAY_HEIGHT (1080)" in the "app_tidl" demo in the vision apps (before was #define DISPLAY_WIDTH (1280) #define DISPLAY_HEIGHT (720)),

    erros happened:

65.788925 s: VX_ZONE_ERROR:[ownContextSendCmd:782] Command ack message returned failure cmd_status: -8
65.789204 s: VX_ZONE_ERROR:[ownContextSendCmd:818] tivxEventWait() failed.
65.789224 s: VX_ZONE_ERROR:[ownNodeKernelInit:526] Target kernel, TIVX_CMD_NODE_CREATE failed
65.789239 s: VX_ZONE_ERROR:[ownNodeKernelInit:527] Please be sure the target callbacks have been registered for this core
65.789254 s: VX_ZONE_ERROR:[ownNodeKernelInit:528] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
65.789272 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 0, kernel com.ti.hwa.display ... failed !!!
65.789290 s: VX_ZONE_ERROR:[vxVerifyGraph:2044] Node kernel init failed
65.789304 s: VX_ZONE_ERROR:[vxVerifyGraph:2098] Graph verify failed
app_tidl: ERROR: Verifying display graph ... Failed !!!

why? The sdk version is "07_02_00_06"

Best Regards

Gong