This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C674x 1.2V and 1.3V CVDD

Other Parts Discussed in Thread: TMS320C6748, AM1808

Hello all,

We're considering making a board with population options to support either the -3 (375MHz) or -4 (456MHz) speed grades of the C6746 or C6748. Since we are not planning on using the RTC or  having a variable core voltage, we had planned on connecting all the 1.2V static and 1.2V core pins together. The C6748 datasheet section 6.3.1 defines the static pins as: RVDD, VDDA_12_PLL0, VDDA_12_PLL1, USB_CVDD , and SATA_VDD. Furthermore we are not using USB or SATA.

I'm confused about which pins on the -4, 1.3V chip must be connected to the 1.3V rail? Here's what I was able to determine so far. Can someone please confirm these are the correct connections? Ideally we'd like to save the extra power supply circuitry and just connect everything to the CVDD rail. Is that permitted?

 

Pin Connection on -4 Chip Reference / notes
RVDD 1.3V Section 3.8.27
PLL0_VDDA 1.2V Section 3.8.2
PLL1_VDDA 1.2V Section 3.8.2
USB_CVDD 1.2V USB not used in application. Section 3.8.17
SATA_VDD No Connect SATA not used in application. For Rev B silicon, can be left disconnected.

I've also used this wiki page as a reference for unused pins: http://processors.wiki.ti.com/index.php/OMAP-L1x_Schematic_Review_Checklist#If_not_used

 

Many thanks,

Mike