Hi all,
Reading through the MCUSW MCAL documentation, being a beginner with TDA4 I was not able to fully comprehend the documentation to the level of implementation. It would be great to help me out in my query or pointing to the right documentation for references to implement the requirement.
1. How to build and flash the example application provided when the Linux kernel running on A72?
2. how can I run the CAN peripheral interface on the safety MCU island and interface it with external sensors?