Other Parts Discussed in Thread: OMAP3530
Hi,
I'm working with an OMAP3530 custom board based on the Beagle C4. The memory I'm working with is the MT29C4G48MAPLCJI-6.
I'm trying to compile a x-loader so I can upload it to the ram via the UART3. I've downloaded the xloader code from git://gitorious.org/x-load-omap3/mainplain.git, and I compiled it with the codesourcery_g++ toolchain.
But I cant't make it properly, every time I upload the x-loader, I can't go into the next step and upload de u-boot (via UART 3 too)
If I use an already compiled x-loader, I've no problem, but I want to modify some code in the x-loader so I need to be able to compile it.
What am I doing wrong?
Any sugestions are accepted!
Thanks.