Hi,
I am using TDA4VMXEVM board.
In pci-epf-test.c file using pci_epf_test_raise_irq() func we are able to generate MSI interrupt from End point to Root Complex
Same way from pci_endpoint_test.c file I want to generate MSI interrupt from Root complex to End point
1. Is it possible to generate MSI interrupt from Root complex to End point ?
2. Any sample source code is available?
3. Does any changes required in DTS file ? if yes what are those changes ?
4. Please let me what are changes required in platform driver files
5. Any other ways we can generate interrupt from Root complex to end point ?
Thanks
Gangadhar