Hello,
I am working on AM/DM37x Mistral EVM, dvsdk_4_01_00_09.
The Linux kernel is Arago/2.6.32-psp03.00.01.06/dm37
The encode demo works fine when I connect a DVD to the board's Composite Input (and audio In port) - both video and audio are encoded.
Can I work with a USB camera?
Does it require a special driver?
The bootargs I am using are
set bootargs 'console=ttyS0,115200n8 root=/dev/nfs nfsroot=10.0.0.3://home/benny/target_omap3730,nolock noinitrd rw ip=dhcp:::off mem=74M mpurate=1000 omap_vout.vid1_static_vrfb_alloc=y omapfb.mode=dvi:720x480MR-16@60 omapdss.def_disp=lcd rootwait'
Regards,
Benny