This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Not recovered from decode error .

We are using "ti-dvsdk_dm365-evm_4_00_00_22" , and decode H264 .

( Decode stream made by DM365 .  (high profile / Level 4 / 1280x720 / 4Mbps / 15fps ) )

 

Causing a packet loss, DecodeErr cause.( Vdec2_process() return Dmai_EBITERROR )

After eliminating packet lossIDR is received.( Vdec2_process() return Dmai_EOK )

But , Decoded image still remains DecodeError . ever after ..

 

I was investigated, perhaps because   IH264VDEC_Params.displayDelay = 1 . 

If IH264VDEC_Params.displayDelay = 16 ,  such a phenomenon does not occur .  ( Recovered error )


Why would not  IH264VDEC_Params.displayDelay = 1 , when DecodeError occurs ?

 

 

thank you .