I have a spectrum digital XDS560v2 travel and just recently stopped working in CCS 7.4 and 9.3 (once and a while I get it to connection); however, no issues when running sd560v2config program. it does work on other computer could a windows update cause this? if so is there a fix? I've turn off antivirus no effect. I do have a XDS200 and BlackHawk usb200 both connect fine the only issue is with the xds560V2.
winver = 20H2
below CCS 7.4 (test connection)
----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Send::dtc_conf
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Send::dtc_conf
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Send::dtc_conf
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Send::dtc_conf
Loaded FPGA Image: C:\ccs7\ccsv7\ccs_base\common\uscif\dtc_top.jbc
The library build date was 'Nov 6 2017'.
The library build time was '09:31:00'.
The library package version is '7.0.100.0'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
SD56v2Config
Spectrum Digital Configuration Utility (running DTC_CONF)
@BEGIN-1
addrConf=:55756
addrIo=:55755
boardRev=2
dtcName=none
epkRev=2.2.0.0
fpgaRev=1.57
ipAddress=none
ipBroadcast=none
ipClient=none
ipConfig=dhcp
ipGateway=none
ipHwaddress=none
ipLeasehours=none
ipLeasetime=none
ipMtu=none
ipNetmask=none
ipNetwork=none
ipPointopoint=none
productClass=XDS560V2
productName=XDS560V2 TRAVELER
safeMode=false
serialNum=00:0E:99:03:D0:A2
swBuildTime=Sep 30 2011 11:26:30
swRev=2.2.0.5
time=none
vendorName=Spectrum Digital
standbyEnable=true
standbyMinutes=20
@END-1
Thanks in advance
Rob