i try to run the example dsk_app.out to hear a voice signal using the aic23 , but when i load the program on ccs4 and connectting the dsk , an error mesasge ( invalid format ) come out
it means the dsk_app.out
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i try to run the example dsk_app.out to hear a voice signal using the aic23 , but when i load the program on ccs4 and connectting the dsk , an error mesasge ( invalid format ) come out
it means the dsk_app.out
ahmed awad,
Welcome to the TI E2E Forums.
Did you re-build dsk_app.out? Or was it already built using earlier tools? Those could be incompatible with CCSv4.
Which version of CCSv4 are you using?
Where did you get the dsk_app.out file and the dsk_app project?
What processor was the original dsk_app example built for?
What else was in the error message? At what point in your connect / load / run process did the error show up? In which window did it show up?
My apologies that I only have questions and not answers.
Regards,
RandyP
thanks any way mr Randy, no worries
i had posted a message again on e2e concerning this problem , my answers to your questions are as follows:
Did you re-build dsk_app.out? Or was it already built using earlier tools? Those could be incompatible with CCSv4.
the dsk_app.out was originally built and i don't know which version of ccs was used but i guess v3.? , i got it from http://c6000.spectrumdigital.com/dsk6455/v2/ after that i made a new project and i copied the content of the dsk_app folder located in the ..........\boards\dsk6455_v2\examples\dsk_app in my project in the workspace , i tried then to build my project i get 6 errors which i took much time trying to fix them..
Which version of CCSv4 are you using?
Version: 4.2.1.00004
Where did you get the dsk_app.out file and the dsk_app project?
http://c6000.spectrumdigital.com/dsk6455/v2/
What processor was the original dsk_app example built for?
actually i don't know what they do use to build the project and got the .out file
What else was in the error message? At what point in your connect / load / run process did the error show up? In which window did it show up?
really sorry for not being able to provide you with a printed screen photo to show you the errors , due to the net speed, but i describe you the errors
after i copied the content of the dsk_app folder into my project in the workspace and build it i get these errors :
the console window is filled with many errors but the problems window tells me the following
[ ***** USER ERROR ***** - ] GBL_config size parameter error.