Part Number: DRA821U
Hi ,
We are trying to use gzip compressed kernel image from TISDK .
Looks like u-boot doesn't support gzip kernel decompression.
| Booting using the fdt blob at 0x90ecf200 Uncompressing Kernel Image gunzip error -5 |
Enabled gzip compression in u-boot configuration ( CONFIG_SPL_GZIP) uncompressing the kernel ok but when u-boot handles control to kernel saw synchronous abort with CPU reset
"Synchronous Abort" handler, esr 0x02000000 elr: 0000000000930000 lr : 00000000808025b4 (reloc) elr: 0000000080008000 lr : 00000000ffeda5b4 x0 : 000000008e8cd000 x1 : 0000000000000000 x2 : 0000000000000000 x3 : 0000000000000000 x4 : 0000000080008000 x5 : 0000000000000001 x6 : 0000000000000008 x7 : 0000000000000000 x8 : 00000000fdead838 x9 : 0000000000000002 x10: 000000000a200023 x11: 0000000000000002 x12: 0000000000000002 x13: 000000000001869f x14: 0000000000000000 x15: 00000000ffed9a58 x16: 00000000fff3b6f4 x17: 00000000fdecfe10 x18: 00000000fdeb7de8 x19: 00000000fffd29b0 x20: 00000000fffaa296 x21: 0000000000000000 x22: 0000000000000001 x23: 00000000fdecf7a8 x24: 00000000fdecf7a8 x25: 00000000fffb9da8 x26: 0000000000000000 x27: 00000000ffeda5f0 x28: 00000000900000d8 x29: 00000000fdead870Code: 5ef7d1fe 956d35fd 035d7d3f e6e4c4ad (464c457f) Resetting CPU ...resetting ... |
Please let me know if I missed any other settings?
Are other versions of compression(zImage) supported ?
Thanks,
Swapna