This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: PM Lib and SCI client interfaces

Part Number: TDA4VM

Hi,

When I checking for the SCI client usages, I could see that /ti/ti-processor-sdk-rtos-j721e-evm-07_03_00_07/pdk_jacinto_07_03_00_29/packages/ti/drv/pm  is implementing some features of Sciclient and it also provides interface to handle many features of SCI client.

I have some basic questions related to this context,

  1. Is it the TI recommended way of handling PM related operations or SCI client/ server / direct can be used always ?
  2. Is there a detailed user guide on how to use these interfaces for TDA4 devices ?
  3. Is there an interface to use  the PMIC TPS6594x for the TDA4 architecture ?