This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with using NFS on DM6446!

U-Boot 1.1.3 (Dec  4 2006 - 12:05:38)                 

U-Boot code: 81080000 -> 81097628  BSS: -> 810A0018
RAM Configuration:
Bank #0: 80000000 256 MB
Flash: 16 MB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 297MHz
DDR Clock :- 162MHz
Hit any key to stop autoboot:  0
## Booting image at 02050000 ...                                               
   Image Name:   Linux-2.6.10_mvl401-davinci_evm                               
   Image Type:   ARM Linux Kernel Image (uncompressed)                         
   Data Size:    1333196 Bytes =  1.3 MB                                       
   Load Address: 80008000                                                      
   Entry Point:  80008000                                                      
   Verifying Checksum ... OK                                                   
OK                                                                             
                                                                               
Starting kernel ...                                                            
                                                                               
Linux version 2.6.10_mvl401-davinci_evm (xlibrary@scarletoak.sanb.design.ti.com6
CPU: ARM926EJ-Sid(wb) [41069265] revision 5 (ARMv5TEJ)                         
CPU0: D VIVT write-back cache                                                  
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets           
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets             
Machine: DaVinci EVM                                                           
Memory policy: ECC disabled, Data cache writeback                              
Built 1 zonelists                                                              
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nM
PID hash table entries: 512 (order: 9, 8192 bytes)                             
Console: colour dummy device 80x30                                             
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)                 
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)                   
Memory: 120MB = 120MB total                                                    
Memory: 118784KB available (2271K code, 480K data, 136K init)                  
Mount-cache hash table entries: 512 (order: 0, 4096 bytes)                     
CPU: Testing write buffer coherency: ok                                        
spawn_desched_task(00000000)                                                   
desched cpu_callback 3/00000000                                                
ksoftirqd started up.                                                          
desched cpu_callback 2/00000000                                                
desched thread 0 started up.                                                   
NET: Registered protocol family 16                                             
Registering platform device 'musb_hdrc'. Parent at platform                    
DaVinci I2C DEBUG: 12:15:02 Aug  1 2006                                        
Registering platform device 'i2c'. Parent at platform                          
usbcore: registered new driver usbfs                                           
usbcore: registered new driver hub                                             
JFFS2 version 2.2. (NAND) (C) 2001-2003 Red Hat, Inc.                          
yaffs Aug  1 2006 12:14:38 Installing.                                         
Registering platform device 'davincifb.0'. Parent at platform                  
Setting Up Clocks for DM420 OSD                                                
Console: switching to colour frame buffer device 90x30                         
fb0: dm_osd0_fb frame buffer device                                            
fb1: dm_vid0_fb frame buffer device                                            
fb2: dm_osd1_fb frame buffer device                                            
fb3: dm_vid1_fb frame buffer device                                            
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled      
Registering platform device 'serial8250'. Parent at platform                   
ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A                                 
io scheduler noop registered                                                   
io scheduler anticipatory registered                                           
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize          
Registering platform device 'ti_davinci_emac'. Parent at platform              
TI DaVinci EMAC: MAC address is 00:0e:99:02:41:5d                              
TI DaVinci EMAC Linux version updated 4.0                                      
TI DaVinci EMAC: Installed 1 instances.                                        
netconsole: not configured, aborting                                           
i2c /dev entries driver                                                        
Linux video capture interface: v1.00                                           
Registering platform device 'vpfe.1'. Parent at platform                       
DaVinci v4l2 capture driver V1.0 loaded                                        
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2                       
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx    
hda: TOSHIBA MK4032GAX, ATA DISK drive                                         
elevator: using anticipatory as default io scheduler                           
ide0 at 0xe10661f0-0xe10661f7,0xe10663f6 on irq 22                             
hda: max request size: 1024KiB                                                 
hda: 78140160 sectors (40007 MB), CHS=16383/255/63                             
 hda: hda1 hda2                                                                
    ide0: BM-DMA at 0xe1066000-0xe1066007, BIOS settings: hda:pio, hdb:pio     
mice: PS/2 mouse device common for all mice                                    
musb_hdrc: version 2.2a/db-0.4.8 [pio] [host] [debug=0]                        
musb_hdrc: USB Host mode controller at c8060000 using PIO, IRQ 12              
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1             
hub 1-0:1.0: USB hub found                                                     
hub 1-0:1.0: 1 port detected                                                   
Registering platform device 'davinci-audio.0'. Parent at platform              
NET: Registered protocol family 2                                              
IP: routing cache hash table of 512 buckets, 4Kbytes                           
TCP: Hash tables configured (established 8192 bind 16384)                      
NET: Registered protocol family 1                                              
NET: Registered protocol family 17                                             
Sending DHCP requests ., OK                                                    
IP-Config: Got DHCP answer from 255.255.255.255, my address is 192.168.0.165   
IP-Config: Complete:                                                           
      device=eth0, addr=192.168.0.165, mask=255.255.255.0, gw=192.168.0.1,     
     host=192.168.0.165, domain=mshome.net, nis-domain=(none),                 
     bootserver=255.255.255.255, rootserver=192.168.0.208, rootpath=           
Looking up port of RPC 100003/2 on 192.168.0.208                               
Looking up port of RPC 100005/1 on 192.168.0.208                               
VFS: Mounted root (nfs filesystem).                                            
Freeing init memory: 136K                                                      
FATAKernel panic - not syncing: Attempted to kill init!                        
L: kernel too ol d

 

 

My U-boot settings

videocfg=video=davincifb:osd0=720x480x16,2025K:osd1=720x480,2025K:vid0=720x480,2025K:vid1=720x480,2025K                                      
bootcmd=bootm 0x2050000                                                                                                                      
bootargs=console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.0.208:/home/lion1988/newworkdir/filesys,nolock mem=120M    
stdin=serial                                                                                                                                 
stdout=serial                                                                                                                                
stderr=serial                                                                                                                                
ethaddr=00:0e:99:02:41:5d                                                                                                                    
videostd=ntsc

 

Help me!