This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6474 I2C Boot

Hello,

We have designed a PCB with 2x 6474's and 1x6455. One of the 6474's is booted from I2C then configure MCBSP as SPI and get extended boot image from SPI FLASH. This works fine. Then DSP gets Main System Load from SPI FLASH and runs. So far Only Core 0 get its load from SPI. I want to download other cores after this procedure is completed but I think when I2C boot is over core 1 and core 2 are released from reset. Am I right with this issue?

Is it possible to keep core 1 and core 2 in reset until core 0 runs and release other cores from reset after some time?

Thanks

Alphan