Part Number: AM6548
Other Parts Discussed in Thread: AM6546, TMDX654IDKEVM,
I try to use DCC on our custom board with AM6546 SR2.0, but can not put anything in the source registers (DCCCLKSRC1 and DCCCLKSRC0).
- Writing to DCCCLKSRC1 and DCCCLKSRC0 always gives 0 in registers
- Writing to DCCGCTRL, DCCCNTSEED0, DCCCNTVALID0 and DCCCNTSEED1 works fine
- It looks like it is the same on all DCCs (DCC0-DCC7 and MCU_DCC0-MCU_DCC2)
- I have tested the same on the evaluation board I have (TMDX654IDKEVM with AM65xx SR1.0). On the evaluation board it is possible to set registers DCCCLKSRC1 and DCCCLKSRC0
- One observation is the DCCREV register. On the RCU601 3.0.0 On the evaluation board: 2.0.4
Best regards
Johnny Mostraum