Other Parts Discussed in Thread: TMS320C6678, LM10010, UCD9222, TPS56121, UCD9244
Hi,
As far as I understand, the smartrelex allow the system to lower the CVDD voltage in order to reduce power, according to the DSP performance.
1. Can I use a fixed 1.1V power supply instead of the smartflex adjustable power supply? (I think it's like class-0 mention in sprabi2) ?
2. If not using the smart flex, can I leave the relevant pins (VCL, VD, VCNTL0-3) floating?
3. If I drive CVDD from the same power supply of CVDD1 (e.g. 1V fixed), what is the degradation in the DSP performances I will get?
4. We are using DSP bios, does smartflex supported in the DSP bios?
4. Erez