Other Parts Discussed in Thread: ADS131E04, TMDXICE110
Hi.
I am using the AMIC110 ICE board to prototype an application. I was wondering if I can use the McASP pinned out to the launchpad connectors for an SPI device. If so, can you provide some example code?
It seems the nearly infinite flexibility of the mcasp would allow it if I could only figure out what to do!
I'm connecting to an ADS131E04 ADC. I also need to connect to an accelerometer, so I was hoping to use both the SPI port and the MCASP port that are on the launchpad connectors.
Thanks!
John