Hi experts,
Is it possible for the C6748 EMIFA to access 32-bits even when the data bus is 16-bits?
In the C6713, when READ/WRITE 16-bit data, the strobe signal goes out twice. If we check the control waveforms, we can see that it is accessing the data twice by switching EMA_BA[1], which gives the image of handling 32bit data. Please let me know if we can do the same with the C6748.
Also, if you have a sample code to evaluate EMIF, it would be helpful.
Best Regards,
O.H