Other Parts Discussed in Thread: OMAP3530, TMS320DM365
Dear Sir
while executing my executable (UNIVERSAL application - my own codec) on the target (Linux/OMAP3530) I got: [1] Failed to open /dev/cmem [2] can't open engine Note1: While I compiled my server I got the following message ""undefined.createMemMapFile(): program = bin/servercom_x64P" - but no error was generated and the executable server was produced. Note2: I deleted SECTIONS{} from packages/gnu/targets/arm/linkcmd.xdt as I was instructed in an earlier psot of mone to bypass CodeSourcery bug that produces ld error 11 (segmentation fault) during the application linking stage Ofer