This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6454 DSP help

We have a good customer in WA that is needing some embedded processor help, please see his request below.

 

Date Opened:          3/22/2011 06:39:19 PM
Company Name:     Medicis Technology
Contact Name:        Randy Holmberg
Contact Phone:        (425) 420-2175
Contact Email:         rholmberg@medicis.com
Address:                  11818 North Creek PKWY
City and State:         Bothell, WA
Postal Code:            98021

 

Gentlemen, Here are some questions regarding our application for the 6454 DSP. Please take a look and let me know if you can help answer the following questions. 1) There is a pin called RSV09 that is connected to DGND on our current board design. In an older version of the 6454 data sheet, it had indicated that this pin could be connected to ground if the EMAC RGMII is not used (we do not use the EMAC). However, we have just noticed that the newest data sheet shows that this pin should be connected to 1.8V. Please let me know what issues we might expect to see with this pin connected to ground as we currently have it. 2) The other question is more of a note on where we are currently at with the HPI32 integration. We have been able to bring the 6454 out of reset, set PLL registers (via host port) and observe correct clock frequencies. However, I do not believe we have access to L2 SRAM and I believe read accesses to other registers within the 6454 are not correct (all zeros). Please let us know if the RSV09 pin connection could cause our Host Port Read access issues. 3) One other question is in regards to the 14 pin JTAG connection. Can you please send me information to purchase the correct JTAG emulator and software (from TI or 3rd party) to help us debug our intended system connections – HPI32 and EMIF. Sincerely, Randy Holmberg

Thank you for your assistance in this.  Lori Hagen

 

  • From one of our factory experts, RSV09 is a reserved DDR2 pin and is not going to affect the Host Port directly.

    The datasheet change is the new recommended usage for new designs, but we do not anticipate a problem on existing designs that have it tied to DGND.

    Regards,
    RandyP

     

    If you need more help, please reply back. If this answers the question, please click  Verify Answer  , below.