Part Number: TMS320C6652
Hi experts,
In the case of C6652, how should I look at "6.25 PLL Boot Configuration Settings" in the datasheet(SPRS841E)?
I have checked "6.25 PLL Boot Configuration Settings" in the datasheet, but in the case of 6652, the internal clock is limited to 600MHz. Currently, the clock input is 100MHz in No boot Mode, so I think the BOOTMODE [12-10] setting is 011, but in reality, it works with other settings. However, the internal clock seems to be different depending on the setting because the DSP surface temperature is obviously different.
I would like to know why the above phenomenon is observed, so I would appreciate if you could give me some information about the behavior of C6652.
Best Regards,
O.H