Part Number: EVMK2G
Other Parts Discussed in Thread: OMAPL138
Hi experts,
For my work I am approaching to EVMK2G. My aim is performing a code by means of the DSP (on L2SRAM).
I downloaded pdk_k2g_1_0_16 and I installed CCS10.2.
Currently I am configuring the interrupts on the timers by means of the OSAL library (bare metal code).
I configured 3 timers with the following settings:
- TIMER1: as timer1 expires the function taskISR is executed on interrupt number 14;
- TIMER2: as timer2 expires the function taskISR2 is executed on interrupt number 13;
- TIMER3: as timer3 expires the function taskISR3 is executed on interrupt number 15.
All the timers are dual unchained low.
Currently my code works fine because as soon as each timer expires, the corrisponding ISR is executed.
However, I am not able to perform the nesting of the interrupts.
Specifically, if the taskISR3 is ongoing, the higher proprity tasks (task ISR and taskISR2) are not executed.
Is the INTC module able to manage nested interrupts on the DSP?
Thank you in advance for your support.
Best regards,
Benito