This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: kernel crashed with log NETDEV WATCHDOG: eth1 (j721e-cpsw-virt-mac): transmit queue 0 timed out

Part Number: TDA4VM

There are kernel crash issue with the follow log,  the full log is attached to this case.  could you please give us some suggestions about it

I found some similar error issue from tie2e, maybe it is useful.

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/979085/am4376-netdev-watchdog-does-not-reset-step-2?tisearch=e2e-sitesearch&keymatch=NETDEV%20WATCHDOG%3A%20eth1%20%28j721e-cpsw-virt-mac%29#

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/192365/am3874-netdev-watchdog-eth0-cpsw-transmit-queue-0-timed-out

Jun 21 15:11:21 sixi-slave kernel: [ 57.139014] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off
Jun 21 15:11:21 sixi-slave kernel: [ 57.139039] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Jun 21 15:11:30 sixi-slave kernel: [ 66.098083] ------------[ cut here ]------------
Jun 21 15:11:30 sixi-slave kernel: [ 66.098091] NETDEV WATCHDOG: eth1 (j721e-cpsw-virt-mac): transmit queue 0 timed out
Jun 21 15:11:30 sixi-slave kernel: [ 66.098136] WARNING: CPU: 1 PID: 0 at net/sched/sch_generic.c:447 dev_watchdog+0x2ec/0x2f8
Jun 21 15:11:30 sixi-slave kernel: [ 66.098137] Modules linked in: usb_storage xhci_plat_hcd xhci_hcd rpmsg_client_sample ti_am335x_adc usbcore omap_rng rpmsg_char kfifo_buf rng_core cdns3 virtio_rpmsg_bus roles udc_core pru_rproc usb_common irq_pruss_intc crct10dif_ce ti_j721e_cpsw_virt_mac icss_iep ti_k3_r5_remoteproc sa2ul ti_am335x_tscadc pruss sha512_generic authenc ti_k3_dsp_remoteproc cdns3_ti rti_wdt sch_fq_codel rpmsg_kdrv_switch ip_tables x_tables ipv6
Jun 21 15:11:30 sixi-slave kernel: [ 66.098172] CPU: 1 PID: 0 Comm: swapper/1 Not tainted 5.4.74-ACU-2.1.1.10 #1
Jun 21 15:11:30 sixi-slave kernel: [ 66.098173] Hardware name: Texas Instruments K3 J721E SoC (DT)
Jun 21 15:11:30 sixi-slave kernel: [ 66.098176] pstate: 40000005 (nZcv daif -PAN -UAO)
Jun 21 15:11:30 sixi-slave kernel: [ 66.098179] pc : dev_watchdog+0x2ec/0x2f8
Jun 21 15:11:30 sixi-slave kernel: [ 66.098182] lr : dev_watchdog+0x2ec/0x2f8
Jun 21 15:11:30 sixi-slave kernel: [ 66.098183] sp : ffff80001002fdb0
Jun 21 15:11:30 sixi-slave kernel: [ 66.098185] x29: ffff80001002fdb0 x28: ffff000848713c80
Jun 21 15:11:30 sixi-slave kernel: [ 66.098187] x27: 0000000000000004 x26: 0000000000000140
Jun 21 15:11:30 sixi-slave kernel: [ 66.098190] x25: 00000000ffffffff x24: 0000000000000001
Jun 21 15:11:30 sixi-slave kernel: [ 66.098192] x23: ffff00085252c41c x22: ffff00085252c000
Jun 21 15:11:30 sixi-slave kernel: [ 66.098195] x21: ffff00085252c440 x20: ffff800010ff1000
Jun 21 15:11:30 sixi-slave kernel: [ 66.098197] x19: 0000000000000000 x18: 0000000000000000
Jun 21 15:11:30 sixi-slave kernel: [ 66.098199] x17: 0000000000000000 x16: 0000000000000000
Jun 21 15:11:30 sixi-slave kernel: [ 66.098201] x15: ffff80001100a000 x14: ffff8000110c74e2
Jun 21 15:11:30 sixi-slave kernel: [ 66.098203] x13: 00000000000073a8 x12: ffff8000110c6000
Jun 21 15:11:30 sixi-slave kernel: [ 66.098205] x11: ffff80001100a000 x10: ffff8000110c6b30
Jun 21 15:11:30 sixi-slave kernel: [ 66.098207] x9 : 0000000000000001 x8 : 0000000000000000
Jun 21 15:11:30 sixi-slave kernel: [ 66.098209] x7 : 0000000000000004 x6 : 00000000000004f6
Jun 21 15:11:30 sixi-slave kernel: [ 66.098211] x5 : ffff00087fa81848 x4 : 0000000000000001
Jun 21 15:11:30 sixi-slave kernel: [ 66.098213] x3 : ffff00087fa81848 x2 : 0000000000000007
Jun 21 15:11:30 sixi-slave kernel: [ 66.098215] x1 : 88b06faecedb5600 x0 : 0000000000000000
Jun 21 15:11:30 sixi-slave kernel: [ 66.098218] Call trace:
Jun 21 15:11:30 sixi-slave kernel: [ 66.098222] dev_watchdog+0x2ec/0x2f8
Jun 21 15:11:30 sixi-slave kernel: [ 66.098227] call_timer_fn.isra.0+0x20/0x78
Jun 21 15:11:30 sixi-slave kernel: [ 66.098229] run_timer_softirq+0x1a0/0x408
Jun 21 15:11:30 sixi-slave kernel: [ 66.098232] __do_softirq+0x120/0x25c
Jun 21 15:11:30 sixi-slave kernel: [ 66.098235] irq_exit+0xb8/0xd8
Jun 21 15:11:30 sixi-slave kernel: [ 66.098239] __handle_domain_irq+0x64/0xb8
Jun 21 15:11:30 sixi-slave kernel: [ 66.098241] gic_handle_irq+0x5c/0x148
Jun 21 15:11:30 sixi-slave kernel: [ 66.098243] el1_irq+0xb8/0x180
Jun 21 15:11:30 sixi-slave kernel: [ 66.098246] arch_cpu_idle+0x10/0x18
Jun 21 15:11:30 sixi-slave kernel: [ 66.098250] do_idle+0xc0/0x140
Jun 21 15:11:30 sixi-slave kernel: [ 66.098253] cpu_startup_entry+0x24/0x68
Jun 21 15:11:30 sixi-slave kernel: [ 66.098256] secondary_start_kernel+0x148/0x180
Jun 21 15:11:30 sixi-slave kernel: [ 66.098258] ---[ end trace e23048f2ad374935 ]---
Jun 21 15:11:30 sixi-slave kernel: [ 66.098267] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0 eth1: txq:0 DRV_XOFF:0 tmo:8960 dql_avail:-350 free_desc:509
Jun 21 15:11:34 sixi-slave kernel: [ 70.962094] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0 eth1: txq:0 DRV_XOFF:0 tmo:13824 dql_avail:-350 free_desc:509
Jun 21 15:11:40 sixi-slave kernel: [ 76.082092] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0 eth1: txq:0 DRV_XOFF:0 tmo:18944 dql_avail:-350 free_desc:509
Jun 21 15:11:44 sixi-slave kernel: [ 80.946092] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0 eth1: txq:0 DRV_XOFF:0 tmo:23808 dql_avail:-350 free_desc:509
Jun 21 15:11:50 sixi-slave kernel: [ 86.066092] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0 eth1: txq:0 DRV_XOFF:0 tmo:28928 dql_avail:-350 free_desc:509
Jun 21 15:11:54 sixi-slave kernel: [ 90.930092] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0 eth1: txq:0 DRV_XOFF:0 tmo:33792 dql_avail:-350 free_desc:509
Jun 21 15:12:00 sixi-slave kernel: [ 96.050094] j721e-cpsw-virt-mac main_r5fss_cpsw9g_virt_mac0 eth1: txq:0 DRV_XOFF:0 tmo:38912 dql_avail:-350 free_desc:509