Hi,
I am working on beagleboard-xm (BBXM) and wish to interface touchscreen LCD panel with it.
It would be very nice if someone could explain how could I do so?
BBXM has expansion connector where SPI port(3 and 4) signals are available. But at present the MCBSP signals (audio) are in use.
How to change the pin muxing in u-boot or kernel to use the SPI interface?
Regards,
Swati Jain