This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EG-17: Is there a patch that can support one VIP bt656 to receive four uyvy cameras

Part Number: TDA2EG-17

Hi

 sdk: ti-processor-sdk-linux-automotive-dra7xx-evm-03_04_00_03 

I need to receive four 720p30fps uyvy data through a VIP interface bt656 and transmit each pixel of four cameras alternately. For example, transfer cam1 1pixes CAM2 1pixes CAM3 1pixes cam4 1pixes? Is VIP supported? Is there a patch that can support one VIP bt656 to receive four uyvy cameras?