Part Number: AM5728
Hello everybody,
I would like to ask you a question if Ti PSDK 6.0 is ready for QT 5.15.
- Powervr: ti-sgx-ddk-km_1.17.4948957: k4.19
- 2a777b8fb72a89d299b82845d42b63b2a2618daa
- OpenGL: ti-sgx-ddk-um_1.17.494857:zeus
- 551665bf9c321bc3e7721416e6ebbc9f65c18155
Everything is running well with QT 5.12.9, but after upgrading to version 5.15 I have an error: "Cannot find EGLConfig, returning null config".
From the QT sources I've founded, that they're just calling libEGL.eglChooseConfig from your library.
EGLConfig QWindowsEGLContext::chooseConfig(const QSurfaceFormat &format)
{
QVector<EGLint> configureAttributes = createConfigAttributesFromFormat(format);
configureAttributes.append(EGL_SURFACE_TYPE);
configureAttributes.append(EGL_WINDOW_BIT);
configureAttributes.append(EGL_RENDERABLE_TYPE);
configureAttributes.append(EGL_OPENGL_ES2_BIT);
configureAttributes.append(EGL_NONE);
EGLDisplay display = m_staticContext->display();
EGLConfig cfg = nullptr;
do {
// Get the number of matching configurations for this set of properties.
EGLint matching = 0;
if (!QWindowsEGLStaticContext::libEGL.eglChooseConfig(display, configureAttributes.constData(), nullptr, 0, &matching) || !matching)
continue;
// Fetch all of the matching configurations and find the
// first that matches the pixel format we wanted.
int i = configureAttributes.indexOf(EGL_RED_SIZE);
int confAttrRed = configureAttributes.at(i+1);
i = configureAttributes.indexOf(EGL_GREEN_SIZE);
int confAttrGreen = configureAttributes.at(i+1);
i = configureAttributes.indexOf(EGL_BLUE_SIZE);
int confAttrBlue = configureAttributes.at(i+1);
i = configureAttributes.indexOf(EGL_ALPHA_SIZE);
int confAttrAlpha = i == -1 ? 0 : configureAttributes.at(i+1);
QVector<EGLConfig> configs(matching);
QWindowsEGLStaticContext::libEGL.eglChooseConfig(display, configureAttributes.constData(), configs.data(), configs.size(), &matching);
if (!cfg && matching > 0)
cfg = configs.constFirst();
EGLint red = 0;
EGLint green = 0;
EGLint blue = 0;
EGLint alpha = 0;
for (const EGLConfig &config : configs) {
if (confAttrRed)
QWindowsEGLStaticContext::libEGL.eglGetConfigAttrib(display, config, EGL_RED_SIZE, &red);
if (confAttrGreen)
QWindowsEGLStaticContext::libEGL.eglGetConfigAttrib(display, config, EGL_GREEN_SIZE, &green);
if (confAttrBlue)
QWindowsEGLStaticContext::libEGL.eglGetConfigAttrib(display, config, EGL_BLUE_SIZE, &blue);
if (confAttrAlpha)
QWindowsEGLStaticContext::libEGL.eglGetConfigAttrib(display, config, EGL_ALPHA_SIZE, &alpha);
if (red == confAttrRed && green == confAttrGreen
&& blue == confAttrBlue && alpha == confAttrAlpha)
return config;
}
} while (reduceConfigAttributes(&configureAttributes));
if (!cfg)
qWarning("Cannot find EGLConfig, returning null config");
return cfg;
}
Output from testing application:
QStandardPaths: XDG_RUNTIME_DIR not set, defaulting to '/var/volatile/tmp/runtime-root'
qt.qpa.egldeviceintegration: EGL device integration plugin keys: ("eglfs_emu", "eglfs_kms_egldevice", "eglfs_kms")
qt.qpa.egldeviceintegration: EGL device integration plugin keys (sorted): ("eglfs_kms", "eglfs_emu", "eglfs_kms_egldevice")
qt.qpa.egldeviceintegration: Trying to load device EGL integration "eglfs_kms"
qt.qpa.eglfs.kms: Loading KMS setup from "/etc/qt5/eglfs_kms_cfg.json"
qt.qpa.eglfs.kms: Requested configuration (some settings may be ignored):
headless: false
hwcursor: false
pbuffers: true
separateScreens: false
virtualDesktopLayout: 0
outputs: QMap(("VGA1", QMap(("mode", QVariant(QString, "off"))("name", QVariant(QString, "VGA1")))))
qt.qpa.eglfs.kms: New DRM/KMS via GBM integration created
qt.qpa.egldeviceintegration: Using EGL device integration "eglfs_kms"
qt.qpa.eglfs.kms: platformInit: Opening DRM device
qt.qpa.eglfs.kms: GBM: Using DRM device "/dev/dri/card0" specified in config file
qt.qpa.eglfs.kms: Using backend-provided DRM device /dev/dri/card0
qt.qpa.eglfs.kms: Creating GBM device for file descriptor 5 obtained from "/dev/dri/card0"
qt.qpa.eglfs.kms: Initalizing event reader for device 0x4c3de0 fd 5
qt.qpa.eglfs.kms: Querying EGLDisplay
...
qt.qpa.eglfs.kms: "UNKNOWN1" mode count: 1 crtc index: 0 crtc id: 55
qt.qpa.eglfs.kms: mode 0 1024 x 600 @ 60 hz
qt.qpa.eglfs.kms: Selected mode 0 : 1024 x 600 @ 60 hz for output "UNKNOWN1"
qt.qpa.eglfs.kms: Physical size is QSizeF(154, 86) mm for output "UNKNOWN1"
qt.qpa.eglfs.kms: Format is 34325258 requested_by_user = false for output "UNKNOWN1"
qt.qpa.eglfs.kms: Output "UNKNOWN1" framebuffer size is QSize(1024, 600)
...
qt.qpa.eglfs.kms: Output UNKNOWN1 can use 4 planes: 35 38 43 48
qt.qpa.eglfs.kms: Chose plane 35 for output UNKNOWN1 (crtc id 55) (may not be applicable)
qt.qpa.eglfs.kms: Using plain OpenGL mouse cursor
qt.qpa.eglfs.kms: No EDID data for output "UNKNOWN1"
qt.qpa.eglfs.kms: Sorted screen list: QVector(OrderedScreen(QPlatformScreen=0x4e1430 ("UNKNOWN1") : 2147483647 / QPoint(0,0) / primary: false))
qt.qpa.eglfs.kms: Adding QPlatformScreen 0x4e1430 ( "UNKNOWN1" ) to QPA with geometry QRect(0,0 1024x600) and isPrimary= false
qt.qpa.input: evdevkeyboard: Using device discovery
qt.qpa.input: udev device discovery for type QFlags<QDeviceDiscovery::QDeviceType>(Device_Keyboard)
qt.qpa.input: Found matching devices ("/dev/input/event0")
qt.qpa.input: Adding keyboard at /dev/input/event0
qt.qpa.input: Try to create keyboard handler for "/dev/input/event0" ""
qt.qpa.input: Opening keyboard at /dev/input/event0
qt.qpa.input: Create keyboard handler with for device "/dev/input/event0"
qt.qpa.input: Unload current keymap and restore built-in
qt.qpa.input: numlock=0 , capslock=0, scrolllock=0
qt.qpa.input: evdevmouse: Using device discovery
qt.qpa.input: udev device discovery for type QFlags<QDeviceDiscovery::QDeviceType>(Device_Mouse|Device_Touchpad)
qt.qpa.input: Found matching devices ()
qt.qpa.input: evdevtouch: Using device discovery
qt.qpa.input: udev device discovery for type QFlags<QDeviceDiscovery::QDeviceType>(Device_Touchpad|Device_Touchscreen)
qt.qpa.input: Found matching devices ("/dev/input/event1")
qt.qpa.input: evdevtouch: Adding device at /dev/input/event1
qt.qpa.input: evdevtouch: Using device /dev/input/event1
Created context for format QSurfaceFormat(version 2.0, options QFlags<QSurfaceFormat::FormatOption>(), depthBufferSize -1, redBufferSize 8, greenBufferSize 8, blueBufferSize 8, alphaBufferSize -1, stencilBufferSize -1, samples -1, swapBehavior QSurfaceFormat::DoubleBuffer, swapInterval 1, colorSpace QSurfaceFormat::DefaultColorSpace, profile QSurfaceFormat::NoProfile) with config:
EGL_BUFFER_SIZE: 24
EGL_ALPHA_SIZE: 0
EGL_BLUE_SIZE: 8
EGL_GREEN_SIZE: 8
EGL_RED_SIZE: 8
EGL_DEPTH_SIZE: 0
EGL_STENCIL_SIZE: 0
EGL_CONFIG_CAVEAT: 12344
EGL_CONFIG_ID: 5
EGL_LEVEL: 0
EGL_MAX_PBUFFER_HEIGHT: 0
EGL_MAX_PBUFFER_PIXELS: 0
EGL_MAX_PBUFFER_WIDTH: 0
EGL_NATIVE_RENDERABLE: 1
EGL_NATIVE_VISUAL_ID: 875713112
EGL_NATIVE_VISUAL_TYPE: 12344
EGL_SAMPLES: 0
EGL_SAMPLE_BUFFERS: 0
EGL_SURFACE_TYPE: 4
EGL_TRANSPARENT_TYPE: 12344
EGL_TRANSPARENT_BLUE_VALUE: 0
EGL_TRANSPARENT_GREEN_VALUE: 0
EGL_TRANSPARENT_RED_VALUE: 0
EGL_BIND_TO_TEXTURE_RGB: 0
EGL_BIND_TO_TEXTURE_RGBA: 0
EGL_MIN_SWAP_INTERVAL: 1
EGL_MAX_SWAP_INTERVAL: 1
qt.qpa.input: evdevtouch: /dev/input/event1: Protocol type B (multi), filtered=no
qt.qpa.input: evdevtouch: /dev/input/event1: min X: 0 max X: 2047
qt.qpa.input: evdevtouch: /dev/input/event1: min Y: 0 max Y: 2047
qt.qpa.input: evdevtouch: /dev/input/event1: min pressure: 0 max pressure: 0
qt.qpa.input: evdevtouch: /dev/input/event1: device name: PenMount PM2203C
qt.qpa.eglfs.kms: Creating gbm_surface for screen UNKNOWN1
qt.qpa.eglfs.kms: Got native format 34325258 from eglGetConfigAttrib() with return code true
Created context for format QSurfaceFormat(version 2.0, options QFlags<QSurfaceFormat::FormatOption>(), depthBufferSize 24, redBufferSize 8, greenBufferSize 8, blueBufferSize 8, alphaBufferSize -1, stencilBufferSize 8, samples -1, swapBehavior QSurfaceFormat::DoubleBuffer, swapInterval 1, colorSpace QSurfaceFormat::DefaultColorSpace, profile QSurfaceFormat::NoProfile) with config:
EGL_BUFFER_SIZE: 24
EGL_ALPHA_SIZE: 0
EGL_BLUE_SIZE: 8
EGL_GREEN_SIZE: 8
EGL_RED_SIZE: 8
EGL_DEPTH_SIZE: 24
EGL_STENCIL_SIZE: 8
EGL_CONFIG_CAVEAT: 12344
EGL_CONFIG_ID: 7
EGL_LEVEL: 0
EGL_MAX_PBUFFER_HEIGHT: 0
EGL_MAX_PBUFFER_PIXELS: 0
EGL_MAX_PBUFFER_WIDTH: 0
EGL_NATIVE_RENDERABLE: 1
EGL_NATIVE_VISUAL_ID: 875713112
EGL_NATIVE_VISUAL_TYPE: 12344
EGL_SAMPLES: 0
EGL_SAMPLE_BUFFERS: 0
EGL_SURFACE_TYPE: 4
EGL_TRANSPARENT_TYPE: 12344
EGL_TRANSPARENT_BLUE_VALUE: 0
EGL_TRANSPARENT_GREEN_VALUE: 0
EGL_TRANSPARENT_RED_VALUE: 0
EGL_BIND_TO_TEXTURE_RGB: 0
EGL_BIND_TO_TEXTURE_RGBA: 0
EGL_MIN_SWAP_INTERVAL: 1
EGL_MAX_SWAP_INTERVAL: 1
Cannot find EGLConfig, returning null config
qt.qpa.eglfs.kms: Adding FB, size 1024x600, DRM format 0x34325258
qt.qpa.eglfs.kms: Setting mode for screen UNKNOWN1
qt.qpa.input: evdevtouch: Updating QInputDeviceManager device count: 1 touch devices, 0 pending handler(s)
qt.qpa.eglfs.kms: Adding FB, size 1024x600, DRM format 0x34325258
qt.qpa.eglfs.kms: Adding FB, size 1024x600, DRM format 0x34325258
What's wrong here?
Thank you,
Andy