This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6455 interrupt issue under DSP/BIOS



HI,DEAR TI,
//----------------------------------
DSP:6455;CCS:3.3.82.13;BIOS:5.41;CGT:6.1.13;NDK:2.0
//----------------------------------
my board also hava a piece of fpga and a ddc,both of them via gpio as interrupt pin link to dsp.
as follow:
fpga--gp8--dsp
in the tcf GUI:
interrupt selection num:59; function:_fpga_isr; use dispatcher;interrupt mask:all
in the tcf GUI:
ddc---gp9--dsp
interrupt selection num:60; function:_ddc_isr; use dispatcher;interrupt mask:all
//-----------------------------------
 in the main()
       IER |= 1<<8; //Enable fpga  interrupt
        IER |= 1<<9; //Enable ddc   interrupt
when running, i can run into ddc_isr and fpga_isr,i want to disable fpga interrupt and ddc interrupt
in ddc_isr,so in the
void ddc_isr() i use
        IER &=~(1<<8)
       IER &=~(1<<9)
to disable ddc and fpga interrupt ,but the ddc and fpga interrupt cannot be disabled.
why? how can i disabled interrupt in isr?
thank you!

  • feng,

    When you return from any interrupt service routine, the expected result is that all status and registers are restored to their original values. This includes IER.

    DSP/BIOS provides an interrupt mask through the HWI_Dispatcher that can choose which interrupts to enable or disable during the execution of the ISR. But IER will be restored to its original value when you return to the point of the interruption.

    My recommendation would be to post a SWI that will execute after the HWI returns, and include an argument to that SWI that indicates which IER bits should be cleared.

    If I do not understand your question, or if these comments do not help or do not make sense, please reply back.

    Regards,
    RandyP

     

    If you need more help, please reply back. If this answers the question, please click  Verify Answer  , below.