Part Number: PROCESSOR-SDK-J721E
Hello,
I have a question about the following timing parameters related to the display:
prm.timings.width = 1920U; prm.timings.height = 1080U; prm.timings.hFrontPorch = 88U; prm.timings.hBackPorch = 148U; prm.timings.hSyncLen = 44U; prm.timings.vFrontPorch = 4U; prm.timings.vBackPorch = 36U; prm.timings.vSyncLen = 5U; prm.timings.pixelClock = 148500000ULL;
These parameters are located in the following file: <SDK_PATH>/vision_apps/apps/basic_demos/app_tirtos/common/app_init.c
My question is if these parameters are initialized only one time through this file or there is a possibility to make changes from the vision apps demos, single cam app for example.
Best Regards,
Mohamed