Part Number: TDA4VM
Hi,
When I used my personal 2 images upload to Edge AI cloud, and run the Edge AI evaluation tools, it reports 1st picture have below warning and can not finish the inference work, could you explain the warning contents and how to solve it? The 2nd images is OK. I attached the original 1st image for your reference.
50%|█████ | 1/2 [00:02<00:02, 2.42s/it]/usr/local/lib/python3.6/dist-packages/ipykernel_launcher.py:10: MatplotlibDeprecationWarning:
Adding an axes using the same arguments as a previous axes currently reuses the earlier instance.
In a future version, a new instance will always be created and returned. Meanwhile, this warning can be suppressed,
and the future behavior ensured, by passing a unique label to each axes instance.

Thanks
Thomas