Part Number: PROCESSOR-SDK-AM335X
Hi
I am trying to understand and install ADB bridge in AM335x starter kit , but on Linux Kernel and not Android OS
I am using the Yocto build and was successfully able to add recipe "android-tools"
I would now like to know , how do I test
1. if my AM335x can be connected to Windows Host and
2. Windows application can use detect the AM335x device as Android devcie
For the above to happen, I guess the Am335x SK should have ADB client and windows should be ADB server