This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How should CCSv4 be configured for a DM3730 on a TMDSEVM3730 (Mistral AM/DM 37x EVM) using Blackhawk XDS-560v2

Other Parts Discussed in Thread: DM3730, OMAP3530

Device: DM3730

Platform: TMDSEVM3730 (Mistral AM/DM 37x - Model TMDXEVM3730) Evaluation Module

Code Composer Studio Version 4.2.1.00004

Emulator: Blackhawk XDS-560v2 USB version Bh560v2Config v.1.0.0.5

I am setting up a CCSv4 project for this EVM. I do not see a DM3730 device option or an option to select this EVM. We tried using OMAP3530 and OMAP3630 as the device but ran into problems. I found the DM3730 GEL files on the TI E2E Wiki. Loading these cleared up connection problems to the ARM Cortex8 core but we still have problems with the DSP core. Before I proceed futher, I would like to check on how to properly set up CCSv4 for this device and EVM.

Is there an update availible to add the DM3730 and/or EVM to CCSv4?

If not, how should CCSv4 be setup? Which device should be selected.

Thanks