Other Parts Discussed in Thread: TMDXIDK5718
Hello everyone,
We are experincing a mistake when we try to launch a simple Hello-world project with our custom board which implement an AM5708 Chip.
The Test connection Pass with an XDS110 USB Debug Probe & the folowing config:
Configuration file
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Texas Instruments XDS110 USB Debug Probe_0">
<instance XML_version="1.2" desc="Texas Instruments XDS110 USB Debug Probe_0" href="connections/TIXDS110_Connection.xml" id="Texas Instruments XDS110 USB Debug Probe_0" xml="TIXDS110_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Texas Instruments XDS110 USB Debug Probe_0">
<instance XML_version="1.2" href="drivers/tixds510icepick_d.xml" id="drivers" xml="tixds510icepick_d.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds510arm9.xml" id="drivers" xml="tixds510arm9.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds510cs_dap.xml" id="drivers" xml="tixds510cs_dap.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds510cortexM.xml" id="drivers" xml="tixds510cortexM.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds510cs_child.xml" id="drivers" xml="tixds510cs_child.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds510c66xx.xml" id="drivers" xml="tixds510c66xx.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds510dap_pc.xml" id="drivers" xml="tixds510dap_pc.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds510cortexA15.xml" id="drivers" xml="tixds510cortexA15.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds510csstm.xml" id="drivers" xml="tixds510csstm.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds510etbcs.xml" id="drivers" xml="tixds510etbcs.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds510pru.xml" id="drivers" xml="tixds510pru.xml" xmlpath="drivers"/>
<property Type="choicelist" Value="0" id="The JTAG TCLK Frequency (MHz)"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="AM5708_0" href="devices/AM5708.xml" id="AM5708_0" xml="AM5708.xml" xmlpath="devices"/>
</platform>
</connection>
</configuration>
</configurations>
Test Connection results:
[Start: Texas Instruments XDS110 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\rbarraud\AppData\Local\TEXASI~1\
CCS\ccs930\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Jan 31 2021'.
The library build time was '20:08:09'.
The library package version is '9.3.0.00042'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG IR Integrity scan-test has succeeded.
-----[Perform the Integrity scan-test on the JTAG DR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Integrity scan-test has succeeded.
[End: Texas Instruments XDS110 USB Debug Probe_0]
We are able to launch the configuration & to connect the main core A-15:

but then we are not able to load the hello world project:

an error occure:
Unable to terminate memory Download:
I guess that the problem is comming from the fact that the memory Adress is not well configurate in the IDE?
Their is some extra confirguration to do before launching a custom project?
Thanks a lot for your answer.