I am currently working with a DSP project built on CCS6 in 2014 and it is using BIOS 6_35_04_50 as well as NDK 2_23_00_00. I was wondering if it would be worth upgrading this project into CCS10 to the use the latest BIOS and NDK versions, if there are any advantages for using CCS10 over CCS6, and what would be the smoothest path to upgrade the project? The BIOS and NDK are running a daemon to create TCP socket connections, currently it has trouble connecting and holding connections.