This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi engineers,
We want to reduce the startup time of SBL, so the focus is on OSPI-CLK, OSPI-DMA, Dcache and Icache. TI's currently released SDK-Does SBL support OSPI to use DMA and Cache? Please tell me the SDK version that supports the above functions. I will conduct a test to see if DMA and Cache can reduce the startup time to meet the needs of our project. Thank you!
HI
SBL does support OSPI DMA. Can you try enabling it?
I did not get question about cache, cache is already enabled for SBL.
Regards,
Brijesh
Please tell me which SDK version support OSPI DMA,now i use the SDK 7.2,and please tell me how to enable DMA,i have found threre are two DMA precompilation conditions,but when i modify them the project can not compiled successfully,so please tell me how to enable DMA,thanks! I have check the cache configuration but i found the dcache is not enable in SDK 7.2 ,please check ,thanks!
in the sbl_component.mk file, there is a flag SBL_USE_DMA, can you set it to yes, rebuild SBL and check it?
Regards,
Brijesh
I have set the flag SBL_USE_DMA,and then I debug an review the OSPI registers,I found the OSPI-DMA bits are not config,I have found a flag which named SPI_DMA_ENABLE,should I turn on this flag?if this flag is useful,please tell me how to enable this flag.
Hi,
Where do you enable SBL_USE_DMA to yes? This flag will internally enable SBL_DMA_ENABLE build macro. So we need to just set SBL_USE_DMA to yes in sbl_component.mk file for the SBL that you are using.
Regards,
Brijesh
Hi,
What command do you use to build SBL? Could you please share it? I will tell you where to change based on this command.
Regards,
Brijesh
Hi,
we use this command: make pdk_libs -j16
make -j BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release sbl_cust_img
Hi,
We did a test according to your suggestion, but the test results show that the DMA has not been turned on successfully. During debugging, it was found that the precompilation condition of SBL_USE_DMA was not turned on, which resulted in the DMA related variables and registers not being configured, as shown in Figure 2 and Figure 3. . The makefile modification items are shown in Figure 1. Is there a problem with the makefile modification? Cause the pre-compilation conditions have not been modified?
Hi,
Can you also make sure that DMA is enabled for cust library and cust image, as shown below?
sbl_lib_cust_MAKEFILE = -f$(PDK_SBL_COMP_PATH)/build/sbl_lib.mk BOOTMODE=cust SBL_USE_DMA=yes CUST_SBL_FLAGS=$(CUST_SBL_TEST_FLAGS)
sbl_cust_img_MAKEFILE = -f$(PDK_SBL_COMP_PATH)/build/sbl_img.mk BOOTMODE=cust SBL_USE_DMA=yes BUILD_HS=no CUST_SBL_FLAGS=$(CUST_SBL_TEST_FLAGS)
Please make sure to rebuild libraries after making these changes, like below
make -s -j4 BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release sbl_lib_cust_clean sbl_cust_img_clean
make -s -j4 BOARD=j721e_evm CORE=mcu1_0 BUILD_PROFILE=release sbl_lib_cust sbl_cust_img
Regards,
Brijesh