Hi All,
Can i use BSP_WINCE_ARM_A8_01_01_00_OMAP35XX_AMDM37XX_Demo in TMDSEVM3730 Development kit?
I am facing a problem in booting TMDSEVM3730 using the BSP_WINCE_ARM_A8_01_01_00_OMAP35XX_AMDM37XX_Demo downloaded from following link
http://software-dl.ti.com/sdoemb/sdoemb_public_sw/wince_sdk/latest/index_FDS.html.
The Same Demo Binary i'm able to download in TMDXEVM3730 using SD boot (SW4: 1 , 2, 3 ON and the remaining are OFF). TMDSEVM3730 in debug port it is showing only 60 when trying SD boot. The Same board is working with the linux/android Demo provided with the kit.
Thanks in Advance
Jethin Sekhar