Hi All,
I have designed AM3356 based OEM module with 256MB RAM (MT41J128M16JT-125). It is working well.
Now we need to upgrade the RAM size to 1GB single chip.
Please refer to the below part numbers and confirm the RAMs are pin to pin replacements for the current 256MB part (MT41J128M16JT-125).
| ISSI | IS43TR16512B-125KBL |
| Alliance Memory | AS4C512M16D3LA |
Also please share the Linux driver correction details 256MB model to 1GB model.
Regards
Anees PK.