Part Number: TDA4VM
Hi,
I am seeing a strange booting behavior on a new TDA4VM EVM:
An EVM that is ready to boot from SDCARD, if Displayport#0 is connected to a monitor and turning the power switch on, the EVM does not boot, the LED LD6 and LD5 do NOT turn on, only LD7 turns on.
If the Displayport#0 is disconnected, the EVM boots correctly and all LED LD7, LD6, LD5 turn on. After the successful boot, hot plugging the Displayport#0 to the monitor works and the display also works.
So this must be a problem at startup maybe during power sequencing.
Is this a known issue?
HW:
PROC078E8A(001)
PROC079E3D
SW:
Linux SDK 7.3 with prebuilt binaries
Regards,
--Gunter