Part Number: DRA829V
Hi
In our custom Board we are using 4GB eMMC we are trying eMMC booting.
so we want to know the offset need to keep for the eMMC as mentioned in the link below is for higher size memory so we not able to write to the block mention below. our maximum block is (0x1000)
boot0 partition (8 MB) user partition 0x0+----------------------------------+ 0x0+-------------------------+ | tiboot3.bin (512 KB) | | | 0x400+----------------------------------+ | | | tispl.bin (2 MB) | | | 0x1400+----------------------------------+ | rootfs | | u-boot.img (4 MB) | | | 0x3400+----------------------------------+ | | | environment (128 KB) | | | 0x3500+----------------------------------+ | | | backup environment (128 KB) | | | 0x3600+----------------------------------+ | | | sysfw (1 MB) | | | 0x3E00+----------------------------------+ +-------------------------+
could you please provide the offset for the u-boot binaries that need to use while flashing.
Regards
Divyanshu