This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6678: memory heap configuration error when using Ethernet boot mode.

Part Number: TMDSEVM6678

I am working on TMDSEVM6678 with processor_sdk_rtos_c667x_6_03_00_106, pdk_c667x_2_0_16
I test the example UART_BasicExample_C6678_c66xTestProject, i worked well when i flash from CCS IDE or boot throught ethernet boot mode.

but the problem happed when i chang the  the line in uart_testcfg file from      "Program.sectMap["systemHeap"]   =   Program.platform.stackMemory;"   to " Program.sectMap["systemHeap"]   =   "DDR3";


follow this thread   https://e2e.ti.com/support/processors-group/processors/f/processors-forum/677010/tms320c6678-ethernet-boot-for-c6678-ddr-config-issue
i see that DDR 3 was not config on the ethernet boot mode so i can understand the problem. But follow the  uart_test.cfg file it still use  "DDR3"  in this section  Program.sectMap[".fardata:benchmarking"].

i try to map it to another memory region like L2SRAM or  MSMCSRAM but it didn't work,  it show the error  " program will not fit into available memory.  run placement with alignment fails for section ".fardata:benchmarking" size 0x4000000", i also comment out it but it still error ( i want to comment out because i see that other project don't need to config it)

// here is a part of uart_test.cfg file

Program.sectMap["systemHeap"]   =   Program.platform.stackMemory;
Program.sectMap[".fardata:benchmarking"] = "DDR3";

So my question is
1. if DDR3 is not config why in config file  setting Program.sectMap[".fardata:benchmarking"] = "DDR3"; it still work?
2. if i keep the config line  " Program.sectMap[".fardata:benchmarking"] "  do have any error when running project, if have how do i resolve it?
3. How can i remove line  " Program.sectMap[".fardata:benchmarking"] "  because i see that other project don't use it?

uart_test.cfg

  • Hi Tung Hoang,

    I have suggestion for question 1, please try this and provide your observation.

    Fullscreen
    1
    2
    Program.sectMap["systemHeap"] = new Program.SectionSpec();
    Program.sectMap["systemHeap"].loadSegment = "DDR3";
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    Will respond to questions 2 and 3 ASAP.

    Thanks,

    Rajarajan