This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64GPEVM: Kernel Loading: Got interrupt data

Part Number: TMDS64GPEVM

Hello 

I'm building YOCTO image for TMDS64GPEVM but the resultant images (base image & default image) both have an issue with kernel loading when running on target.

Kernel prints error message "mmc1: Got data interrupt 0x00000002 even though no data operation was in progress." several times and there is no further messages printed.

This issue was also seen in the pre-built images from the SDK.

Attached below the complete log file obtained.

[Note]: Also used 16GB SD card instead of 8GB but the issue persists.

Kind regards

Mohamed Fathi