This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 SPI problem

Hi,

I'm developing IP camera(DM365) with VA(Video Analytics) module(DM6435).

The communication between DM365 and DM6435 is performed using SPI.

After enabling DM365 SPI in kernel compile option(make menuconfig), after booting that kernel, there is no /dev/spidev* device file. Why?

My kernel version is 2.6.18 and DVSDK version is 2.10.01.18.

Booting logs are the followings.

 

04000000-0x07000000 : "area"
nand_davinci nand_davinci.0: hardware revision: 2.3
MUX: initialized SPI0_SCLK
MUX: initialized SPI0_SDO)
MUX: initialized SPI0_SDI
MUX: initialized SPI0_SDENA0
dm_spi.0: davinci SPI Controller driver at 0xc5066000 (irq = 42) use_dma=0