This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Several questions

Part Number: TDA4VM

Hello,

I plan to use TDA4EV processor and I have looked through the source code of the vision apps and have several quesitons for it

1. How can I setup I2C, I'm going to do multiplexing CSI2 ports (two) with 8 cameras. 

2. Is it possible to do that in the stereo vision app so that I can modifiy the capturing frames and switch between cameras

3. In most camera apps there is a parameter num_frames = 10000, I would like to capture frames continously from the Camers is that possible ?

4. I downloaded the RTOS SDK for getting vision apps, but the processor SDK Linux platform doesn't have vision apps...why ?