This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA718: configure display to switch from Landscape mode to Portrait mode

Part Number: DRA718

Hello TI team,

We are using custom Dra71x processor on our custom board with 6.00.00.03 SDK of Dra7xx EVM.

We require 2 HDMI ports, but this processor supports only one HDMI.

So we have incorporated LT8168EX IC which converts the RBG to HDMI format and inputs to the HDMI connector to the display

This LT8618EX is as i2c slave.

Currently we are able to get the image on the 5.5 inch touch Display but in the Landscape mode, but we required it to be in the Portrait Mode

Can you pls guide us in DSS where we can change the settings so that we can configure to the desired mode.