Other Parts Discussed in Thread: OMAP3530
Hi,
I encounter a problem with the "Chipselect" pins on SPI3 bus on
OMAP3530.
When I use CS0, it works perfectly, but when I try to use CS1, the
corresponding
pin
is always on low level (chipselect activated).
I configured both CS0 and CS1 pins with same options, as following
on uboot :
evm.h
MUX_VAL(CP(ETK_D0_ES2 ), (IEN | PTD | DIS | M1)) /*SPI3_MOSI*/\
MUX_VAL(CP(ETK_D1_ES2 ), (IEN | PTU | EN | M1)) /*SPI3_MISO*/\
MUX_VAL(CP(ETK_D2_ES2 ), (IDIS | PTU | EN | M1)) /*SPI3_CS0*/\
MUX_VAL(CP(ETK_D3_ES2 ), (IEN | PTD | DIS | M1)) /*SPI3_CLK*/\
MUX_VAL(CP(ETK_D7_ES2 ), (IDIS | PTU | EN | M1)) /*SPI3_CS1*/\
Since there is still a difference, I tried to configure in the
kernel with the following lines :
board-omap3evm.c
static struct omap_board_mux board_mux[] __initdata = {
...
OMAP3_MUX(ETK_D2, OMAP_MUX_MODE1 | OMAP_PIN_INPUT_PULLUP |OMAP_PIN_OFF_INPUT_PULLUP | OMAP_PIN_OFF_OUTPUT_HIGH ),
OMAP3_MUX(ETK_D7, OMAP_MUX_MODE1 | OMAP_PIN_INPUT_PULLUP | OMAP_PIN_OFF_INPUT_PULLUP | OMAP_PIN_OFF_OUTPUT_HIGH),
...
once again, CS0 works fine, but CS1 keeps low level at any time.
There is no MUX conflict with other pins, so I don't understand
where is the mistake.
Thanks for your help,
Regards.