Part Number: PROCESSOR-SDK-J7200
Hi TI
For J7200 evm ,CAN-Ethernet gateway demo
Can-Eth-User_Guide.md (ti.com)
We have finished the OSPI flash for tiboot3.bin, tifs.bin, app_switch2.appimage and nor_spi_patterns.bin.
Also make the following settings on the evm board, UART J45/J43 are also connected to evm board
SW8 = 01000001 SW9 = 00011000
After booting, there is no log output to the console. It seems that the program did not start successfully.
Is there anything else to set?