Other Parts Discussed in Thread: DRA821,
Hi team,
On DRA821 EVM, we failed to boot from SD card.
We are using enet_nimu_example which is in PDK as a base.
The program which I want to run on DRA821U access to RTI and MCSPI2 register.
Of course the original example file can run successfully, but the program image which I added the 2 features listed above can't boot from SD card.
However, the modified program can boot from direct load via CCS.
I have no idea to explain this, please help us.
Environment:
bios_6_83_02_07
pdk_j7200_07_03_00_29 (これのenet_nimu_exampleをベースに作成しています。)
ti-cgt-arm_20.2.0.LTS
xdctools_3_61_04_40_core
Best Regards,
Junpei Kishi