This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

zmodem for TeraTerm <-> DM6467T transfer over serial console?



I've been poking around a lot, and haven't found a good solution yet, not even nearly-ready-to-use sourcecode.  I'm approaching a deadline and unfortunately cannot spend more time on this myself.

I wonder if someone out there has the expertise and time to put together the info I've gathered into a usable program for the DM6467T EVM or related boards?

I find source code that includes zmodem (and other protocols) at http://www.ohse.de/uwe/software/lrzsz.html

What's needed is the ability to talk to the EVM using TeraTerm.  That's on the console at 115200 8N1, to be clear.  To be consistent with other lrzsz use, it would be nice to type on the console into the EVM prompt a command such as "sz capturedimage.tif" and then on TeraTerm use command File/Transfer/Zmodem/Receive, and then get the capturedimage.tif transfered over the same console connection up to the host running TeraTerm.  Similarly, "rz revisedprogram" would allow one to send a new program to the EVM, without having to have all the development setup, such as NFS or CCS.

Might someone volunteer to create this DM6467T application?  (I guess, in source code form, it could subsequently run on almost any TI ARM, or any ARM at all.)

ALTERNATIVELY, if something usable is already out there, please let me know!

Thanks,

Helmut