Part Number: BEAGLE-3P-BBONE-AI
Hi Team, seeking for your assistance on this concern.
Working with a beaglebone black using the am335x chip when i build the files in order to boot my device they get tagged making the boot image files be named something other than u-boot zImage and boneblack, after i bitbake and go to look at the files so i can transfer to an sd card in order to boot this is using the beagle bone black
zImage--5.4.58+gitAUTOINC+c5e5dc4e13_706efec4c1-r0-beaglebone-yocto-20210716153001, u-boot-beaglebone-yocto-2020.01-r0, MLO-beaglebone-yocto-2020, am335x-boneblack--5.4.58+gitAUTOINC+c5e5dc4e13_706efec4c1-r0-beaglebone-yocto-20210716153001
those are the names of the files i would be using to boot off the sd card but they seem to be getting tagged. i have the original files , but they are shortcuts to the files named above so i cannot copy/ paste them
Thank you very much.
-Mark