This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't capture 720p input on DM365 EVM board



Hi,

I have got a DM365 EVM board with dvsdk 2_10_01_18.

When i run test "encode -v test.m4v -y 3", only a dark blue screen is output and saved. I have connect a DVD player to evm board. If i don't connect DVD, encode will output "Fail to detect video standard, video input connected?". So, I think connect is correct. And when i connect the DVD player to a TV set, display is also ok.

When i run test "encode -v test.m4v -y 2" and connect video single, all is ok.

Why is 720p fail?

Thx in advance!