This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Load capacitance of the I2C1 and EMIFA lines of the OMAP L138 processor

In our design we have 3 slaves connected to I2C1 and 3 peripherals are connected to EMIFA bus. In order to do the AC analysis I am searching for the maximum driving capacitance(i.e. Load Capacitance) of the I2C1 and EMIFA Bus in the OMAP L138 Datasheet. But unfortunately I am not able to find these Load Capacitance values. Can anyone please help me to get these Load Capacitance values of the I2C1 and EMIFA lines of OMAP L138.

 

Thanks and Regards,

Dinesh Guni